AXIS#.VL.GEARRATIO

Description

This command sets the gain between the position loop compensation (AXIS#.PL.KP and AXIS#.PL.KI ) and the velocity loop. In most applications this value should be equal to 1.0. This gain is most important when using a dual loop configuration when there is a disparity between the position loop scaling and velocity loop scaling. These gains are needed to scale the loops to achieve optimal performance.

Versions

Action Version Notes
Implemented 02-14-03-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 65536.0

Default Value

1.0

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.